How can we help you today?

Can Unity run in a virtual machine

Issue
Can Unity run in a virtual machine

Product Line
Unity

Environment
Windows 7, Windows 10.

Resolution
Unity Pro V13.1 has been successfully tested in the following configuration :
  • VirtualBox 5.1.30 r118389 and 5.2.0-118431
  • VMware Workstation 12 Pro 12.1.0 build-3272444

Note:

If Unity is installed on a virtual machine., the VM must be able to access the Internet.   During the install process, Unity will need access to the
Internet in order to download specific Microsoft Visual C++ Redistributable components.  If these components fail to get installed, Unity will
have problems.