Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the ATV930 drive have a traverse control function embedded?
Issue:
Is traverse control function a built-in feature on the ATV930?

Product Line:
Altivar 930

Environment:
All

Cause:
N/A

Resolution:
Traverse control is not available in ATV930 drive.  This function is only available in ATV320.