Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between EBO SmartDriver and Smart Connector?
SmartDriver and Smart Connector enhance the openness for EcoStruxure Building operation "EBO" BMS system. They enable integration between EBO and 3rd party systems, even via not supported or nonstandard protocols.

SmartDriver:
SmartDriver enables you to create a customized interface to monitor and control 3rd party devices from EBO server.
The following block diagram shows a SmartDriver Interface and a SmartDriver Driver. The SmartDriver Interface (similar in concept to other protocol interfaces such as Modbus and BACnet) is part of EcoStruxure Building Operation software and enables you to create SmartDriver objects in the System Tree pane. The SmartDriver Driver is installed on the server drive and provides the network communications control. More information at Web Help SmartDriver Overview.
Licensing:
Currently, all SmartDrivers are created by the engineering group in the UK. All pricing, installation and licensing will be handled through that office. The ASCII driver does not require any licenses; it is a tool for users to create their own interfaces.

Smart Driver
Smart Connector:
A development framework that simplifies and accelerates integrations with third-party systems or other data sources. It is an open, extensible and configurable application framework that allows developers to create innovative new capabilities, applications, and solutions which extend and enhance EcoStruxure Building solutions.
The Smart Connector itself runs outside the EBO server and consume or server data to EBO server vie the EcoStruxure web services "EWS".

Smart Connector

For more information, visit the Smart Connector marketplace and Developer Community on the Exchange:
https://community.exchange.se.com/t5/SmartConnector/ct-p/smart-connector

For developers wanting to get started using the Smart Connector framework visit:
https://www.smartconnectorserver.com

Licensing:
For deployment: Order part number SXWSWSCDL100001, then download Runtime 2.4 (Commercial) from https://www.smartconnectorserver.com/Marketplace + The cost of Smart Connector itself as defined by the developer.
For Developers: Download Runtime 2.4 (Developer) free; This license allows Extension Developers the ability to install and use the Schneider Electric Smart Connector Runtime for up to 90 days on their development machine. If the license expires, you should download a new license.