Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PME 9.0 - New 3rd party device created with DTE does not work
Product Line
Power Monitoring Expert 9.0

Environment
DTE - Device Type Editor

Issue
The new devices created with DTE are not loading and you will see error messages in the System Log:

"Translator map file 'DEVICE_NAME.xml' not loaded due to previous error. Will retry."
"The attribute 'TimestampedByPlugin' on this element is not defined in the DTD/Schema." -
(or some other attribute as well)

Cause
The modbus-schema.xml file in the config/translator folder is an old version and does not contain the specific attribute referred by the error log.

Resolution
Replace the modbus-schema.xml file in config/translator with the one from system/translator folder or from a healthy PME system.