Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why I am not able to download my application in HMIG2U or HMIG3UX using Ecostruxure Machine Expert V1.1?

Issue

UsingEcostruxureMachine Expert V1.1, the customer mayobservesome difficulties to download his application in HMIG2U and HMIG3UX

Product Line

HMIGU2, HMIG3UX

Environment

EcostruxureMachine Expert

Resolution

With Machine Expert V1.1 , to download an application in HMIG2U or HMIG3X boxes , it is mandatory to do before a download of the last version of Run-time with theRunTimeinstaller tool ofVijeoDesigner.”