This article shows the correct way of licensing the local ViewX client by using the client license method :
As per the previous screenshot, the number of "ViewX Clients"- in this example - is Zero. This means you will not be able to activate remote clients connected to this server unless purchasing a separate valid license, However you can activate the local ViewX client that is installed in your local machine hosting your Geo SCADA server.
Please follow these steps :
- Click the Windows Start Menu, highlight EcoStruxure Geo SCADA and select Configure Connections.
- Click on the 'Properties' button from the right side and make sure that your Geo SCADA Client Configurator has the "Use Client Licensing" option is checked, Then click Ok
- Back to The Geo SCADA Exper 'Client Dialog' again - Click on the 'Licenses' button:
- The following screen will appear:
- Click the browse button and browse to the same file used to activate the server.
- Select file and click open.
- Click on "Apply". The license mode should now show as "File based client license" and validity is "valid".
- Click on the OK button and close the 'Client Licensing' dialog.
- (Re)start the ViewX client by clicking the ViewX icon on your desktop.
Note : If the Machine ID does not appear in Step 4 or Step 8, make sure the Geo SCADA License
Server service is running.
Released for: Schneider Electric Nigeria