Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to set PID feedback assignment to Analog terminal in ATV310?

Parameter Reference channel 1 (401) must not set to 01, only to (163,164 or 183) so that parameter PID feedback assignment (59.00) can be changed from 00 to 01.
This is because you cannot use analog terminal for both reference and feedback at the same time.

1

2