Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to set the output frequency to show on the ATV320 display every time drive is powered on?

Article available in these languages: Czech

Issue:
Change the default display for when the drive is powered on to show output frequency.

Product Line:
Altivar Machines, Altivar 320

Environment:
All models and serial numbers

Cause:
Default display is Reference Frequency

Resolution:
Go to Non (1.2 Monitoring) menu, select rFr (output frequency), and press and hold ENT for more than 2 seconds.  Display will flash to indicate the change had been made.
To dispaly amperage: Go to NON > select NNO > LCr, ENT for more than 2 seconds

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings