Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the outgoing email address of a PM5500 meter?
Issue
The outgoing email address of the meter needs to be white-listed on the network in order to have security access to send emails.

Product Line
PM5500

Environment
Email subscriptions, SMTP server

Cause
The network firewall will not allow the meter's IP address access to the network to send emails, unless the email address is known and can be white-listed.

Resolution
The address that sends out the email is "DoNotReply@SchneiderElectric.com". However, simply white-listing the meter's IP address rather than the generic email address is preferred. With the current firmware version (V2.7.4), the PM5500 does not have a re-configurable email address.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings