Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
To do what, is used the mechanical thermostat NSYCCOTHO with blue button?
To cool the inside of an enclosure by blowing fresh outside air into the enclosure using a fan.
This mechanical thermostat has an open contact.
When the temperature inside the enclosure exceeds the set point, the contact closes and a fan starts.
This implies that the outside air is colder than the set point T °.