Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the VW3A1111 rating for IP66 outdoor?

Issue:
Can the VW3A1111 be used for IP66 rating outdoor?

Product Line:
Altivar Machines, VW3A1111

Environment:
VW3A1111

Cause:
N/A

Resolution:
The VW3A1111 is rated for IP65, and not for IP66 outdoor.