Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the rated short circuit making capacity value Icm for NSX circuit breakers?
NSX breakers are complying to IEC 60947-2.
The rated short-circuit making capacity of a circuit-breaker is the value of short-circuit making capacity assigned to that circuit-breaker by the manufacturer for the rated operational voltage at rated frequency and at a specified power factor for a.c., or time constant for d.c. It is expressed as the maximum prospective peak current.

Based on this standard,clause 4.3.6.1.,for a.c. the rated short-circuit making capacity of a circuit-breaker shall be not less than its rated ultimate short-circuit breaking capacity, multiplied by the factor n of Table 2 (attached)

Schneider Electric Nigeria

Attachment(s)
Table 2.png [78.96 KB]