1. Issue
The customer wants to know if the CANopen Communication DTM is available and operational for the BMECXM0100 module on M580 platform.
The customer wants to know if the CANopen Communication DTM is available and operational for the BMECXM0100 module on M580 platform.
2. Product Line
BMECXM0100
Unity Pro / EcoStruxure Control Expert
BMECXM0100
Unity Pro / EcoStruxure Control Expert
3. Environment
CANopen CommunicationDTM version 1.1.2 (identified on this version, also valid for previous and next versions)
CANopen CommunicationDTM version 1.1.2 (identified on this version, also valid for previous and next versions)
4. Resolution
No, the CANopen Communication DTM is not designed to operate with M580 and with BMECXM0100, but the CXM Master Gateway DTM helps configuring the BMECXM0100 and provides a first level of configuration and diagnostic of the devices.
To configure, adjust, control and monitor the drives and motor control devices, use SoMove software.
No, the CANopen Communication DTM is not designed to operate with M580 and with BMECXM0100, but the CXM Master Gateway DTM helps configuring the BMECXM0100 and provides a first level of configuration and diagnostic of the devices.
To configure, adjust, control and monitor the drives and motor control devices, use SoMove software.
Released for: Schneider Electric Nigeria