Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the cause of SoMove error 1006 connected to the ATV320 drive?

Issue:
SoMove error 1006 on SoMove Software while connecting to the ATV320 drive

Product Line:
ATV320

Environment:
All serial numbers

Cause:
Customer could not connect to the ATV320 drive using SoMove Software getting error 1006.

Resolution:
Error 1006 is an invalid configuration file which means the somove ATV320 DTM file is missing or the imported Somove PSX program does not match the drives part new drives part number, option card etc.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings