Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why do some inverters (VFDs) needs a reactor at the input or DC choke in the DC bus?

In order to smooth the current a choke can be placed upstream the inverter 2 locations possible:

  • In the DC bus
  • Onto the main supply
Choke
Effect of the choke
  • The efficiency of the choke on harmonics is depending on its impedance
  • Higher the impedance, lower the harmonic distortion
  • But higher the impedance, higher the drop voltage