Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
I declared a DDT in which the BOOL Type variable is consuming 2 registers of Address in Unity Pro. Why is that ?
This is the Normal Behavior when you create DDT Data types and assign %MW to a BOOL Variables Because %MW is 32 BITs so it will reserve 2 words.
IN DDT variables either we create all variables as BOOL and in this case, we can use %M   Or all variables as DINT (32 BIT) and in this case, we can use %MW

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings