Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What can cause Vijeo Designer Runtime message: Load Runtime Operation Failed?

Issue
A "Load Runtime Operation Failed" message appears when I launch Vijeo Designer Runtime on a Windows PC or iPC. How do I recover from this situation?

Product Line
Vijeo Designer Generic PC Runtime for Windows (part number VJDSNRTSPC)

Environment
HMI Runtime application on Windows 7 or Windows 10

Cause
When this is seen, it could mean that an improper Windows power-down may have occurred that has corrupted the installation or Windows registry for Vijeo Designer Runtime.
A re-installation of Vijeo Designer Runtime will need to be performed. See below.

Resolution
First, run the Vijeo Designer Registration Wizard to see if it shows the Reference and Serial Number.
If it does, then a reinstall should fix the issue and you will not have to re-register.
The location of the Registration Wizard is:
"C:\Program Files (x86)\Schneider Electric\Vijeo-Designer 6.2\Vijeo-Runtime\Registration\RegistrationWizard.exe"

If it doesn't have a Serial Number, then you will need to find your original serial number which came with the original purchase to re-register the product


1) If you do not have the original project file for Vijeo Designer Configuration software (typically exported as .VDZ extension file), back up the folder "C:\Program Files (x86)\Schneider Electric\Vijeo-Designer 6.2\Vijeo-Runtime\Public\Projects\"
2) Find out the version of Vijeo Designer by right-clicking on "C:\Program Files (x86)\Schneider Electric\Vijeo-Designer 6.2\Vijeo-Runtime\Public\Bin\Koohi.exe"
3) Go Properties, then the "Details Tab"
4) Observe the File Version.
5) Re-install Vijeo Designer Runtime of the same version (call Schneider Electric Support if you need help obtaining the version required)
6) Move the backup files from Step 1 back to the same place (or open and download the (.VDZ) project from Vijeo Designer Configuration software).
7) Run Vijeo Designer Runtime

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings