How can we help you today?

How to Write Workbench I5P File into SCADAPack E-Series RTU?

How to Write Workbench I5P File into SCADAPack E-Series RTU?

The I5P file is a package containing the files needed to load the project. The I5P file is located in the project folder.
Please follow the steps below to write I5P application file to the RTU:


1- You will find the I5P file in a subfolder that has the same name as your Workbench project, If you didn’t find the I5P file in the project, build the project from the project level or the solution level to generate the network configuration files.
Img1


2- Make sure the Device is connected and the logic is Cleared before you go to IEC 61131-3 and select Write Application
Img2


3-Browse your local disk to the folder with the I5P file then Click Open
Img3


4- A confirmation message like below will pop-up
Img4


6- Refresh IEC-61131-3 for the Application Status page
Img5

Schneider Electric Nigeria