Issue
After I've installed Unity Pro v13.x, where do I find the Registration Wizard tool?
Product Line
Unity Pro 13.x for Modicon PLC configuration software for Windows
Environment
Configuration software installed in Windows 7 or above.
Resolution
If you are running on Windows 7 or 8, the icon may be found in the Start Bar in the folder path with a light blue icon:
Schneider Electric -> SoCollaborative -> Unity Pro -> Registration Tool
If you're running Windows 10, you may have difficulty finding the Registration Wizard from the Start Bar.
The file location is:
<Unity Pro InstallFolder>\RegUpXL\RegistrationWizard.exe
If you've installed in the default location, it would be the direct path:
C:\Program Files (x86)\Schneider Electric\Unity Pro\RegUpXL\RegistrationWizard.exe
Note: EcoStruxure Control Expert v14.0 and above uses the newer shared Schneider Electric License Manager Tool.
It is located in the default install location:
C:\Program Files (x86)\Schneider Electric\License Manager\LicenseManager.exe
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Released for: Schneider Electric Nigeria