Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to extend the communication distance to more than 15km between hot standby M580
  1. Issue
Customer would like to set up a hot standby M580 CPU on site. The distance between hot standby M580s is about 30km. But after checking the manual, the maximum distance is only 15km by using fiber-optic SFP transceiver 490NAC0201.

Since that how to extend the maximum communication distance between hot standby M580 more than 15km?
  1. Product Line
M580, 490NAC0201

  1. Environment
None
  1. Resolution
We confirm that it’s feasible to add optical fiber repeaters to extend the maximum communication distance. It’s recommended to select the optical fiber repeaters with large bandwidth capacity.
Additionally, customer need to check whether the synchronized bit of MAST/FAST/SAFE works correctly.