{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Power Monitoring Expert v9.0 and v2020: In few PME installations, flickering is observed in Vista screens contains Numerical Objects which are used to display real-time data values.
Issue
It appears that Vista screens flickering while updating real-time data for the PME version 9.0 and 2020 in some of the systems.

Environment
PME - Thick Apps > Vista


Resolution
*Warning: Take backups of any files prior to modifying/replacing them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop).

Find attached Hotfix "Vista_PME9.zip" which will fix issue in PME v9.0 and the Hotfix “Vista_PME2020.zip” will fix issue in PME v2020.

Download relevant PME version file and unzip the file and copy it in to PME install path '\Schneider Electric\Power Monitoring Expert\system\bin'.

Schneider Electric Nigeria

Attachment(s)
Vista_PME9.zip [1.48 MB]
Vista_PME2020.zip [1.48 MB]