Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Easergy P5 Virtual Injection: How can I enable the virtual injector in eSetup Easergy PRO?
The virtual injection functionality is available only on-line, when the device is connected to a PC using a USB cable. Then the virtual injection window will appear on the right-hand side of Easergy Pro screen.

After connecting to your relay and logging in with Easergy PRO, the user needs to change the mode of the device to ‘Test’ or 'TestBlocked.'