Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to create a device profile in Power SCADA Operation (PSO)

Issue
A new set of devices is getting integrated into the system, but there is no device profile set up for the device type.

Product Line
Power SCADA Operation 9.0

Power Scada Operation 2020

Power Scada Operation 2020 R2

Power Scada Operation 2021

Ecostruxure Power Operation 2022

Ecostruxure Power Operation 2024



Environment
PSO Server, Profile Editor

Resolution

  1. Open Power SCADA Studio and navigate to the Topology page. Open the Device Profile Editor located on the far right.
  2. Select the Define Device Type Tags tab, and hit Add / Edit.
  3. Select Create New, choose a Device Type Name and the desired Category/Subcategory. Make sure the Driver is the correct protocol.
  4. Move the desired tags from the Tag Library over to the Selected Tags list. Save & Exit once complete.
  5. Edit the register information by selecting the Edit... under the Edit Address column. Once the register details are filled out, hit OK.
  6. Repeat step 5 for each tag.
  7. Open the Create Device Profiles tab in Profile Editor and hit Add / Edit next to the Device Profile.
  8. Select Create New, hit Next, choose a Device Profile Name, and hit Next again.
  9. Find the device type that was defined in step 3 and move it over from the Available Devices list to the Selected Devices list and then hit Next.
  10. Select the desired tags that to be included in the project by highlighting and moving them with the arrow button. Once complete, hit Next.
  11. Define whether each tag is PC Based or Trend, and check off any Driver Parameters desired. Hit Finish. The device profile is now created and can be added to the project by following FA404306.