How can we help you today?

Is it possible to having FTP data publishing more frequent that 1 hour on the COM’X 510?

Issue
Is it possible to having FTP data publishing more frequent that 1 hour on the COM’X 510?

Product Line
COM’X510

Environment
FTP Data Pushing

Cause
The maximum default option for FTP data publishing interval is 1hour, but a shorter interval is needed.

Resolution
There is no a way to publish more frequently than once an hour. The available Publication frequency are: Every hour, Every 2 hours, Every 3 hours Every 4 hours, Every 12 hours, Every day, Every week, and Every month.

Schneider Electric Nigeria
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings