Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Connexium Tofino Firewall LSM support
Issue
Available Connexium Tofino Firewall LSMs

Product Line
TCSEFEA23F3F22

Environment

Connexium Tofino Firewall

Resolution
The New LSMs for the Schneider Electric Connexium Tofino firewall TCSEFEA23F3F22 are below:
TCSEFM0002 - ConneXium Tofino DNP3-LSM v3.2
TCSEFM0003 - ConneXium Tofino IEC104-LSM v3.2
TCSEFM0004 - ConneXium Tofino GOOSE-LSM v3.2

And unfortunately, the Schneider Electric Connexium Tofino firewall does not support the NetConnect LSM.