Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you migrate DLF-3000 configuration to another computer?

Issue
User is migrating to a new computer and would like to migrate all the DLF-3000 configuration they have done to the new computer.

Product Line
DLF-3000

Environment
Software Migration

Resolution
The configuration files for DLF 3000 are stored in the following file path C:\DLF-3000\Database (note this path is specified when the software is installed and may vary). To transfer the configuration of DLF 3000, copy/replace the two DLFSystem database files over to the new computer in the same file path. Below is a screenshot showing which files need to be copied over to the new computer.

DLFSystem files

Refer to this article for how to install DLF-3000: https://www.se.com/us/en/faqs/FA203831/