Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
In EcoStruxure Control Expert V14.1, AS-i profiles added in the Private family of BMXEIA0100 configuration screen are not created in the catalog
1. Issue

In EcoStruxure Control Expert V14.1, AS-i profiles added in the Private family of BMXEIA0100 configuration screen are not created in the catalog.

2. Product Line

EcoStruxure Control Expert V14.1, BMXEIA0100
3. Resolution

If folders "V1", "V2" and "V3" do not exist in the "Private" folder under the following path, the user has to manually create them.
C:\ProgramData\Schneider Electric\Control Expert 14.1\ConfCatalog\Database\Asi\Private

AS-i profiles can then be created in the Private family from the BMXEIA0100 configuration screen.

This behavior is fixed in EcoStruxure Control Expert V15.0.