Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which of the Device Types in PME require a Device License?

Issue
Which Devices Types that are added in PME require a Device License?

  • Physical connected devices
  • Devices created with Device Type Editor (DTE) or Modbus Device Importer (MDI)
  • Logical devices


Product Line
Power Monitoring Expert 7.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Power Monitoring Expert 2024

Environment
Floating License Manager
License Configuration Tool

Resolution

Device TypesLicense required
Physical DevicesYes
Device Created with Device Type Editor (DTE) or Modbus Device Importer (MDI) Yes
Logical DevicesNo

Note 1:

  • The license types (E, M, S) are for locales (countries other than the US, Canada, and India) where individual licenses are sold. For locales (the US, Canada, India) where license bundles are sold, a device license is valid for any device type.
  • Device License per Device Type
    • E = Entry-Range Device License
    • M = Mid-Range Device License
    • S = High-End Device License

Note 2:

  • At least one device license must be activated in the system for PME to be able to communicate with a device.
  • Drivers created with DTE or MDI require mid-range (M) type device licenses.
  • Logical devices are not included as devices in the device licensing count.

For more information regarding device types in PME and related licenses, please refer to the Default device type support section in the PME System Guide.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings