Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is maximum number of IEC61850 devices that can be supported by one BMENOP0300 module ?

Dependent on module's mode, the maximum number of IEDs differs :

As Client > max. number of supported IEDs is 32

As Server > max. number of simultaneous client connections is 16 (connection numbers is independent on the number of existing clients. One client could establish more than one connection with the module. Thus, 16 connections do not imply the existence of 16 clients)

For more info, please refer to the attachment

Schneider Electric Nigeria

Attachment(s)
BMENOP.pdf [651.63 KB]