How can we help you today?

How can we adjust the contrast of the display in Easergy MiCOM P63x relays?

Issue/description:

Adjust the contrast of the display in Easergy MiCOM P63x relays

Product family:

Easergy MiCOM P63x relays

Resolution:

The contrast of the display can be adjusted by pressing 3 keys on the local control panel at the same time, as follows:

Please Keep the Enter key and the Clear key pressed simultaneously, then you can press “Up” or “Down”  arrrow to raise or lower the contrast, respectively.