How can we help you today?

How to Logout at the Easergy Micom P63x relay properly ?

Issue/description:

Logout at the Easergy Micom P63x realy  properly

Product family:

Easergy Micom P63x

Resolution:

For security consideration, it would be better to logout the IED once the configuration is done.
The user can be logged out with 'HMI Logout' in the menu tree: 'Par/Conf/CS' or using the softkey 'LOGOUT'.

Additional info.to Logout at Easergy Studio:

Right-click on the device name and select Log Off.
● In the Log Off confirmation dialog click Yes.

Schneider Electric Nigeria