Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Current Limit range for ATS48 Softstarter?
Issue:
What is the minimum and maximum setting for Current Limit on ATS48 Softstarter?

Product Line:
ATS48, Altistart 48

Environment:
All

Cause:
NA

Resolution:
It is adjustable from 150 to 700% of In setting. However, maximum is limited to 500% of rated softstarter current.