Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do all Altivar drives have the DC Bus Terminals?
Issue:
Customer asking if all Altivar Drives have DC Bus Terminals

Product line:
Altivar Drives

Environment:
all

Cause:
Would like to know if the Altivar Drives have DC Bus Terminals

Resolution:
The Altivar 320, 340 and 900 series have DC bus terminals which has the PA+ and PC- for the DC bus voltage. PO or PB or PBe terminals can be used, if needed, for a braking resistor, as shown in each drive's Installation Manual.  The ATV600 Series PA+ and PC- terminals are strictly for measuring DC Bus voltage levels.