Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is Self-healing for capacitors?

Self-healing is a process by which the capacitor restores itself in the event of a fault in the dielectric which can happen during high overloads, voltage transients, etc.
When insulation breaks down, a short duration arc is formed (figure 1)

cap1
The intense heat generated by this arc causes the metallization in the vicinity of the arc to vaporise (figure 2).
cap2

Simultaneously it re-insulates the electrodes and maintains the operation and  integrity of the capacitor (figure 3).
cap3