Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does the [ION_Data]- MAINTENANCE-Job task do under Windows Task Scheduler?

Issue
What does the [ION_Data]- MAINTENANCE-Job task do under Windows Task Scheduler?

Product Line
Power Monitoring Expert (PME) 7.2.x
Power Monitoring Expert (PME) 8.x
Power Monitoring Expert (PME) 9.x
Power Monitoring Expert (PME) 2020
Power Monitoring Expert (PME) 2021
Power Monitoring Expert (PME) 2022
Power Monitoring Expert (PME) 2023
Power Monitoring Expert (PME) 2024


Environment
PME Software

Resolution
image of maintenance job

The ION_Data Maintenance job runs a powershell script which performs a defragmentation on ION_Data.  Details of the script can be found in
Program Files (x86)\Schneider Electric\Power Monitoring Expert\config\cfg\DbScheduledTasks

Note: For large databases the function can take a long time to run which can slow down data insertion so at times it would be disabled to avoid this issue.

Schneider Electric Nigeria

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: