Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the recommended type of Ethernet cables to be used by M580 and Quantum ERIO?

Issue
What is the recommended type of Ethernet cables to be used by M580 and Quantum ERIO?

Product Line
Modicon M580, Quantum, x80 Modules

Environment
BMEP586040, BMECRA31210

Resolution
Schneider Electric has guidelines when making cables connections between remote I/O devices on a Quantum and M580 EIO installation. It is recommended to use shielded twisted pair CAT5e  (10/100 Mbps) cables that complies with TIA/EIA-568 standard and IEC11801 /  EN 50173 class D to protect against the most severe disturbance.

You can find this information on the documents below: