Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to clean and disinfect HMI products such as programmable displays and industrial computers?
Issue
How to clean and disinfect HMI products such as programmable displays and industrial computers?

Product line / Environment
Harmony HMI and iPC

Resolution
Our touch panel can be disinfected using a commercially available alcohol (such as ethanol) disinfectant.
Do not spray the disinfectant directly on the display, but soak it on a soft cloth and wipe it slowly.
* It can be used in the same way even if the environmental protection cover is used.

However, please note the following points:
  • Please pay attention to the precautions of the disinfectant used and the usage environment.
  • Do not use thinner, benzene, organic solvents and strong acidic substances.
  • To protect the touch sheet, do not rub the edge part strongly.