Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to avoid a HALT on Simulator on Win 7 ?
Issue
Some application of Unity Pro Simulator is not working. After a RUN, the application goes to HALT.

Product Line
Unity Pro 13.1

Environment
Windows 7 SP1

Resolution
To avoid this wrong behavior, you have to disable AVX support. You can do that by running this command from an elevated command prompt and then rebooting:
bcdedit /set xsavedisable 1