How can we help you today?

How do you configure logging data to a CSV file in EcoStruxure Machine Expert?

Issue
How do you configure logging data from a Symbol to a CSV file in a EcoStruxure Machine Expert PLC like M241, M251 or M262?

Product Line
EcoStruxure Machine Expert
Modicon M241, M251, M262 Programmable Logic Controllers

Environment
PLC Configuration Software - Logic Builder

Resolution
To configure logging data to file in EcoStruxure Machine Expert, follow these steps:
1) In Logic Builder of your project, go to the Tools tree
2) Right-click on the Application node of your PLC
3) Add a DataLogManager node. This will automatically add the SE_DataLogging library to the Library Manager of this controller
4) Under the DataLogManager node, add a LogFile node. The name that is assigned to this node will be the filename of the log file (e.g. "MyLogFile.log").
In this node, you can choose the storage location (Internal Flash or SD Card), add date and time stamps, choose the maximum entries in the file, choose to use a circular buffer or not, and use a deliminating character for CSV format.
5) In a POU subroutine, add the LogRecord function block from the SE_DataLogging library
6) Name it the same as the LogFile node's name (MyLogFile)
7) Add a LogRecord.Dump, again with the same instance name (MyLogFile)
8) Tie the xDone output pin of the LogRecord block to the xExecute input pin of LogRecord.Dump
9) Assign the variable that you wish to log to the wsRecord input pin of the LogRecord block.
Note that an Integer or Floating point value must be converted to WSTRING type to be logged. This can be done with an INT_TO_WSTRING or REAL_TO_WSTRING conversion operator, for example, respectively.
10)  A rising edge to the xExecute input pin of the LogRecord block will cause the file to be written to.

The file can be accessed by the following steps:
1) Log in to the PLC
2) From the Devices Tree, double-click on the name of the Controller (MyController by default)
3) Go to the Files tab
4) On the right-pane, click the refresh button (spinning green arrows icon)
5) Open the "Log" folder from the PLC. There, you will see the log file.
6) On the left pane, select a destination folder on your PC
7) Click the [<<] button to move the file to your PC. This file can be renamed and opened as CSV in Excel for example.

For more information, please see EcoStruxure Machine Expert - Data Logging Functions - DataLogging Library Guide

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)