Issue
Considerations when using ION setup with V3.0.0 Firmware on ION900, PM8000, and ION7400 meters
Product
ION Setup
ION9000, ION7400, PM8000
Environment
ION9000, ION7400, or PM8000 meter with v3.0.0 firmware
Cause
Changes to the security in v3.0.0 firmware for HEP meters makes old versions of ION Setup not work
Resolution
Recommend a minimum version of ION Setup V3.2.20218.01 when interacting with HEP meters with v3.0.0 firmware.
When trying to load a standard security file, .scf, on a v3.0.0 HEP meter, ION Setup will display the following message
Firmware only supports Advanced Security but can still support a single Standard Login
Selecting Yes will disable the (Legacy Security Support), selecting No will enable (LSS).
Q: With advanced security, is the user name case sensitive ?
A: No, the user name is not case sensitive however certain options are not accepted; USER01, USER 01, USER 1, USER00001
Released for: Schneider Electric Nigeria