Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the correct 3.3V Power Budget for the BMXDRA0815 module?
Issue
The BMXDRA0815 modules 3.3V Power Budget is incorrect in Control Expert 14 and 14.1.


Product Line
M580
BMXDRA0815


Resolution
The correct 3.3V Power Budget for a BMXDRA0815 is 40ma.

It is incorrectly calculated and displayed as 100ma in CE14 and 14.1.

This issue is corrected in Control Expert version 15.