Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
how to create a Web Dsigner application for the BMENOC0311 Factorycast module.

Issue
The purpose of this video is to demonstrate how to create a Web Designer application for the BMENOC0311 Factorycast module. The video also demonstrates how to create the Unity export file that is required for importing the variables into the Web Designer application during development. The user must be familiar with using both Unity and Web Designer.

Product Line
BMENOC0311

Environment
Windows 10

Resolution
The purpose of this video is to demonstrate how to create a Web Designer application for the BMENOC0311 Factorycast module. The video also demonstrates how to create the Unity export file that is required for importing the variables into the Web Designer application during development. The user must be familiar with using both Unity and Web Designer.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings