Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Unity14-UnityLL984 Library install returns ObjectStore error
Issue
Unity14-UnityLL984 Library install returns ObjectStore error

Product Line
Control Expert 14

Environment
Windows 10

Resolution
Installingt the 'UnityLL984 Library' into Control Expert 14, returns the following ObjectStore error.
efr

To resolve the issue:
  • Unzip and run the attached batch file named 'UpdateRegistry'.
  • Install the 'UnityLL984 Library'.

Schneider Electric Nigeria

Attachment(s)
UpdateRegistry.zip [886 Bytes]