Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to solve the Green screen/virtual screen issue ?

Issue

How to solve the Green screen/virtual screen issue ?

Sometimes, after a box wake up, a green screen can be displayed.



This is a virtual screen created by the Intel HD graphic as a extended desktop (the wallpaper can be different)

Product Line

Magelis HMIBMP IPC box

Environment

Win10 RC6.4

Resolution

Update the card graphic driver in v15.40 (or more):
Intel Graphic Driver v15.4

Schneider Electric Nigeria

Attachment(s)
Green_Screen.png [69.71 KB]