Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the BMXERT1604T be synchronized without IRIG-B and DCF77 source in a M580 project ?

1.Issue

Can the BMXERT1604T be synchronized without IRIG-B and DCF77 source in a M580 project ?

2.Environment

M580 series

3.Resolution

The BMXERT1604T with Firmware version >=SV2.0 could be synchronized by M580 Standalone CPU via Xbus by selecting CPU/CRA head as externel clock source.
User needs to select BMXERT1604.2 during hardware configuration .

The clock sync source needs to be CPU/CRA head




Detailed compatibility matrix is shown as below






Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings