Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
If i forgot SP-C-WEB admin password, Can I reset it?
If the administrator's password on a SP-C-WEB controller has been lost, the controller will need to have the programming reset by defaulting the controller. Once the controller has been defaulted a programming backup can be restored.
A programming backup cannot be taken without an administrator password so it is recommended to regularly backup the SP-C-WEB programming.