Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is type of PTC signal coming from motor to ATS22 softstarter?
PTC thermistors are resistors with a positive temperature coefficient, which means that the resistance increases with increasing temperature.
resistance is recognized by soft starter and activates the relevant protection accordingly (Tripping: between 2700 ohm and 3100 ohm).