Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Transfer of project to NOE v6.4 using Web Designer 3.2
Issue
Transfer of project to NOE v6.4 using Web Designer 3.2

Product Line
BMXNOE0110

Environment
Web Designer, Windows 10

Resolution
If you try to transfer an older Web Designer project into a BMXNOE0110 module
(exec firmware version 6.4 and higher) using Web Designer version 3.2,  it will fail
to open the Transfer Status window.

This video will demonstrate how to resolve the issue.