Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to recover the HMIST6xxx if it is in broken mode
  1. Issue
How to recover the HMIST6xxx if it is in broken mode?

  1. Environment
HMIST6xxx.
  1. Resolution
If the HMIST6xxx is in broken mode, user can follow below steps to recover it.

Step1:Select FileSystem and download the project into an USB memory stick.

Step2: Insert the USB memory stick into the HMIST6xxx.
Step3: Click the USB button in below picture.


Then download the selected project to the HMIST6xxx.


Wait for a moment, the HMIST6xxx will be recoverd.

  1. FAQ Applicable Conditions
FAQ applies to HMIST6xxx.