Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many electrical equipment can be connected to Smartlink ELEC?

The quantity of electrical equipment depends on the electrical installation and system architecture.
Smartlink ELEC can connect up to
• 7 digital channels, per channel you can connect to 1 Ti24 auxiliary or 2 pulse energy meters
• 1 analog channel, per channel you can connect to 2 sensors with 4-20mA or 0-10V output.